Skip to main content
MFrat.2
Associate
May 10, 2022 4:13 PM UTC
Question

Why can't my STM32F469 hardware enumerate correctly USB sticks?

Hi all.

I have a hardware with STM32F469, running FreeRTOS and USB stack as configured from CubeMX.

I have the following problem.

I have a preproduction stock of this hardware and 2 USB sticks.

Let's consider only 2 of the above boards (let them be A and B).

Both sticks are correctly enumerated and initialized by board A.

While only one stick of the two works on board B. The other one gets stuck

in enumeration phase.

This thing is driving me crazy.

Any suggestions?

Regards,

Marco

This topic has been closed for replies.

6 replies

Paul1
Senior III
May 10, 2022 4:50 PM UTC

Add delays when starting USB to allow USBStick to stabilize (Some have slower ICs inside than others, or larger capacitors).

  • Delay before enable VBUS power (~100msec).
  • Delay between enabling VBUS and accessing USB Device (~2000msec)

Actual delays required will depend on power source impedance, switches on usb power, circuit capacitance, and sticks used.

Paul

Pavel A.
May 10, 2022 8:17 PM UTC

Test on another board. Not all boards are created equal.

Walid ZRELLI
Visitor II
May 11, 2022 8:49 AM UTC

Hello @MF.2ratini​ ,

This is probably a hardware problem. You could try another board.

BeST Regards,

Walid

MFrat.2
MFrat.2Author
Associate
May 11, 2022 1:30 PM UTC

Hello all and thanks for your contributions.

On this board I have VBUS always ON and have the stack dealing with USB device initialization.

The same USB stick works on 99 boards over 100, while the other works on all boards (just as statitstics). It may be a mix of HW and SW timings at edge, or something similar...

Have no idea yet.

Tesla DeLorean
Guru
May 11, 2022 3:27 PM UTC

Clocking from HSE, HSI or HSI48 ?

USB has tight clock expectations.

A lot of USB Flash drives and CDC can be relatively sloppy.

Perhaps measure the ppm for the internal clock via the MCO PA8 pin routing.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
May 11, 2022 8:16 PM UTC

Bad solder joints toward the USB connector? Incorrect parts? Damaged connector?

Continuity meter and oscilloscope are the basic tools here.

JW