Skip to main content
BMače.1
Visitor II
November 3, 2020
Question

Where to route the external ETH PHY interrupt signal, so it would be used as sub-interrupt in the MAC peripheral?

  • November 3, 2020
  • 0 replies
  • 461 views

The part I am using it the STM32H753II. Trying to use the MAC peripheral I got stuck at PYH interrupt, for which is stated to be included as one of the sub-interrupts of the module (last bullet of 58.8.3). The corresponding mask and status bits are well documented in register description (58.11.4). I have trouble finding information about the way this signal is routed into the device. The PHY interrupt signal is declared as one of the interface signals (58.3), however I fail to find a mapping to the pin of the device, or some other way to define it.

This topic has been closed for replies.