Skip to main content
NYou.1
Associate II
Aug 16, 2021 8:11 PM UTC
Solved

Where to find UCPD1_CC2 pin definition? USB-PD with only CC1 pin?

Hi there. It appears that the STM32G0B1KET LQFP32 MCU lacks a UCPD1_CC2 pin. For this reason I have a couple questions.

  • Can another pin be set to something that will function the same as the UCPD1_CC2 pin?
    • Can UCPD_DBCC1 and UCPD_DBCC2 be used for normal USB-PD functionality aside from dead-battery support?
  • Can USB-PD be implemented with just the UCPD1_CC1 pin?

This topic has been closed for replies.
Yohann M.
Yohann M.Best answer
ST Employee
Aug 17, 2021 6:14 AM UTC

Dear @NYou.1​ 

A application like STM32G071B-DISCO is clearly an application which can be done with 1 CC line.

UCPD_CC1 line is directly connected to the CC line available in the cable.

Regards,

Yohann

3 replies

TDK
Aug 16, 2021 9:03 PM UTC

You can't assign CC2 to another pin. Since it's not exposed, you can only do things that do not require use of that pin. Seems like you need both CC pins for USB-PD.

"If you feel a post has answered your question, please click ""Accept as Solution""."
NYou.1
NYou.1Author
Associate II
Aug 16, 2021 10:38 PM UTC

So I guess the question becomes: What can we do with the UCPD_CC1 Pin? What is the purpose of only having one?

Yohann M.
Yohann M.Best answer
ST Employee
Aug 17, 2021 6:14 AM UTC

Dear @NYou.1​ 

A application like STM32G071B-DISCO is clearly an application which can be done with 1 CC line.

UCPD_CC1 line is directly connected to the CC line available in the cable.

Regards,

Yohann