Skip to main content
This topic has been closed for replies.
PHsi.1
PHsi.1Best answer
Associate II
Jan 30, 2023 7:37 PM UTC

I did find the demo firmware source code under \en.stsw-stm32082\STM3210E-EVAL_FW_V2.1.0 folder.

Thank you very much for your help!!

5 replies

ST Technical Moderator
Jan 30, 2023 7:34 AM UTC

Hello @PHsi.1​ and welcome to the Community :)

You will find the applications of the STM3210E-EVAL board in the STM32CubeF1 MCU package:

STM32Cube_FW_F1_V1.8.4\Projects\STM3210E_EVAL\

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
PHsi.1
PHsi.1Author
Associate II
Jan 30, 2023 3:49 PM UTC

Thank you. I found the ..\applications and ..\examples sub-folders under ..\STM3210E_EVAL with various project folders, such as ..\ADC...,..\FreeRTOS.. etc.

However, I do not know which project folder contains the source code for the "demo program" that was already installed on the EVAL board

PHsi.1
PHsi.1AuthorBest answer
Associate II
Jan 30, 2023 7:37 PM UTC

I did find the demo firmware source code under \en.stsw-stm32082\STM3210E-EVAL_FW_V2.1.0 folder.

Thank you very much for your help!!

Tesla DeLorean
Guru
Jan 30, 2023 8:27 PM UTC

The original one was definitely part of the SPL rather than HAL libraries.

The HAL / CubeF1 has a broader set of examples.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ned.
Associate III
Apr 15, 2023 2:04 AM UTC

Thanks to all; I really find it difficult to find this kind of software.

Cheers, Peter Kelly. ​