Question
When using the STM32 Discovery kit IOT node, I am getting the following error " network interface can not be started"
I recently purchased the kit and was using it for first time yesterday. Initially i didnt get the error, I also tried the Wifi-HTTP server example and it worked, but later when i flashed the aws bin file, i started getting this error. Now even going back to the Wifi-HTTP server example also throws similar error. Is the hardware gone bad, if so what could be the reason, since i was using only the example codes