Skip to main content
BNage.2
Associate
May 5, 2022
Question

When programming a virgin STM32L4 MCU through dfu-util 0.9, it won't exit dfu mode until power cycle.

I am working on a IoT product with the STM32L412CBU6 that requires flashing and testing at our manufacturer. I am able to program the device through DFU mode over USB using:

sudo dfu-util -a 0 -i 0 -s 0x08000000:mass-erase:force:leave -R -D firmware.bin

However, it does not enter back into regular mode. Even if I return the boot pin to low and reset, it still appears as a DFU device with lsusb. However, when I power cycle the device it behaves as if it has the new firmware, and I am able to update the firmware with the exact same script and set it to normal/DFU mode using the boot pin and reset.

My question is why does the dfu update work in EVERY other instance other than the very first time I flash the firmware?

This topic has been closed for replies.

6 replies

Bob S
Super User
May 5, 2022

Probably this http://www.efton.sk/STM32/gotcha/g44.html documented by @Community member​  :)

BNage.2
BNage.2Author
Associate
May 6, 2022

Thanks for the insight. I am going to look into programming the option bytes. It looks like dfu-util has this as an option.

waclawek.jan
Super User
May 6, 2022
MM..1
Super User
May 6, 2022

Why dfutil? STM32Programmer is better for this. And DFU protocol have command for run application , maybe this jump to app work.?

BNage.2
BNage.2Author
Associate
May 6, 2022

I have to use the DFU protocol because that is the interface we selected in product development for updating firmware. I will investigate if the STM32Programmer can run on arm through the USB.

MM..1
Super User
May 7, 2022
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.7.0-RC1
 -------------------------------------------------------------------
 
 
Usage :
STM32_Programmer_CLI.exe [command_1] [Arguments_1][[command_2] [Arguments_2]...]
 
 
Generic commands:
 
 -?, -h, --help : Show this help
 -c, --connect : Establish connection to the device
 <port=<PortName> : Interface identifier. ex COM1, /dev/ttyS0, usb1,
 JTAG, SWD...)
 USB port optional parameters:
 [sn=<serialNumber>] : Serial number of the usb dfu
 [PID=<Product ID>] : Product ID. ex: 0xA38F, etc, default 0xDF11
 [VID=<Vendor ID>] : Vendor ID. ex: 0x0389, etc, default x0483
 UART port optional parameters:
 [br=<baudrate>] : Baudrate. ex: 115200, 9600, etc, default 115200
 [P=<parity>] : Parity bit, value in {NONE,ODD,EVEN}, default EVEN
 [db=<data_bits>] : Data bit, value in {6, 7, 8} ..., default 8
 [sb=<stop_bits>] : Stop bit, value in {1, 1.5, 2} ..., default 1
 [fc=<flowControl>] : Flow control
 Value in {OFF,Hardware,Software} ..., default OFF
 Not supported for STM32MP
 [noinit=noinit_bit]: Set No Init bits, value in {0,1} ..., default 0
 [console] : Enter UART console mode
 JTAG/SWD debug port optional parameters:
 [freq=<frequency>] : Frequency in KHz. Default frequencies:
 4000 SWD 9000 JTAG with STLINKv2
 24000 SWD 21333 with STLINKv3
 [index=<index>] : Index of the debug probe. default index 0
 [sn=<serialNumber>]: Serial Number of the debug probe
 [ap=<accessPort>] : Access Port index to connect to. default ap 0
 [mode=<mode>] : Connection mode. Value in {UR/HOTPLUG/NORMAL/POWERDOWN
}
 default mode: NORMAL
 [reset=<mode>] : Reset modes: SWrst/HWrst/Crst. Default mode: SWrst
 Reset mode with UR connection mode is HWrst
 [shared] : Enable shared mode allowing connection of two or more
 instances of STM32CubeProgrammer or other debugger
 to the same ST-LINK probe.
 [tcpport=<Port>] : Port used for running ST-Link Server, default 7184
 SPI port optional parameters:
 [br=<baudrate>] : Baudrate.
  1. STM32_Programmer_CLI.exe -c port=usb1 -g