Skip to main content
SBach.4
Associate II
July 29, 2023
Solved

when are the commands in the bootloader application notes used?

In the Application Note for the ST Bootloader, DFU bootloader commands such as DFU_DNLOAD are specified. Where would I, as a programmer, use these commands? When communicating with the STM32 microcontroller using the ST Programmer via the command line, I have different commands. Does this mean the ST Programmer is an Application that uses that commands for its communication with the MC bootloader?

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
July 29, 2023

> Does this mean the ST Programmer is an Application that uses that commands for its communication with the MC bootloader?

Of course it is.

1 reply

Pavel A.
Pavel A.Best answer
July 29, 2023

> Does this mean the ST Programmer is an Application that uses that commands for its communication with the MC bootloader?

Of course it is.