Skip to main content
SWint.2
Visitor II
Jun 18, 2021 4:21 PM UTC
Question

What could cause a boot delay of 1-2s on 4/300 boards using STM32F7?

Hi,

We are using STM32F7 in our GUI board and we are experiencing an issue with 4 boards out of 300 where the processor is taking a longer time than usual to boot up. We have measured the time from when the board receives power to when the processor has powered up using an oscilloscope.

On a working board, the time is ~0.5s. On the failing 4 boards, it is 1-2s.

I have checked the errata documentation, reference manual and datasheet but I have not found anything which could explain this problem yet.

Does anyone have any ideas what could cause this boot delay?

Thanks in advance.

Sian

This topic has been closed for replies.

5 replies

TDK
Jun 18, 2021 4:32 PM UTC

It's almost certainly the case that the processor begins executing code (almost) immediately after power-up and something in your program is causing the slowdown. Toggling pins in various stages of the boot-up process helps immensely with tracking down the cause.

One thing that comes to mind is if it's waiting for a clock to be stable, or waiting for another chip to begin communicating correctly.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
Jun 18, 2021 4:56 PM UTC

+1 HSE Not starting (see also LSE, PLL)

Might also be weary of VCAP pins/caps

>>Toggling pins in various stages of the boot-up process helps immensely with tracking down the cause.

Processor is viable at Reset Handler, code some quick assembler code to enable GPIO clocks in RCC, and config/output some pins.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Chief
Jun 18, 2021 5:06 PM UTC

Look for bad soldered pins, resultiing in floating pins.

waclawek.jan
Super User
Jun 18, 2021 7:29 PM UTC

> to when the processor has powered up

What is "processor has powered up"?

JW

Tesla DeLorean
Guru
Jun 18, 2021 8:10 PM UTC

Assumption here is beyond, SystemInit(), main() entry, then SystemClock_Config() and HAL_Init() to start doing anything, so those would be candidates for closer inspection.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..