Skip to main content
Associate II
August 12, 2024
Question

Websocket connection to a public domain through wiznet 5500 and stm32f103

  • August 12, 2024
  • 2 replies
  • 1293 views

Hi,

 

I've been trying to find something on WebSocket connections to a public domain for sending and receiving data for the past month, but couldn't find anything related to Cubeide or C library for WebSockets or the public domain, all I can see are codes associated with Arduino IDE for WebSocket which straight forward uses simple functions, Can Anyone help me with c code for the WebSocket connection to the public domain.

I have initialized the w5500, static/dynamic IP allocation, I can send or receive data through the local network on a local IP address and I can create a socket server on stm32 to receive and send data locally.

 

This topic has been closed for replies.

2 replies

ST Employee
August 20, 2024

Hello @anonymous_stm,

You can find a WebSocket provided by Azure RTOS here, which is free to use on STM32 microcontrollers.

 

With Regards,

"If your question is answered, please close this topic by clicking ""Accept as Solution""."
Andrew Neil
Super User
August 20, 2024

@anonymous_stm wrote:

all I can see are codes associated with Arduino IDE for WebSocket which straight forward uses simple functions


If it's all straightforward & simple, why not just use it?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.