Skip to main content
kiichi
Associate III
Jan 22, 2024 3:30 AM UTC
Question

[version-going-backwards] error occurs when running bitbake.

 

When I add a debug log to the source code, a [version-going-backwards] error occurs.

ERROR: weston-cube-4.0+gitAUTOINC+cd44839e95-r0 do_packagedata_setscene: QA Issue: Package version for package weston-cube went backwards which would break package feeds (from 0:4.0+git0+cd44839e95-r0.1 to 0:4.0+git0+cd44839e95-r0.0) [version-going-backwards]

 

What should I do so that an error does not occur even if I add a debug log?

This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
Apr 22, 2024 9:10 AM UTC

Hi @kiichi ,

I assume that this question remains without answer because there is not enough details.

If you still facing an issue, could you please provide more details about used firmware and compiler also the steps you followed.

If you have already identified the solution, please share it with our Community. That would be helpful for others.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.