Skip to main content
Gil1
Associate II
Oct 31, 2025 5:46 PM UTC
Solved

Using ThreadX Version 6.1

Hi All,

I am using ThreadX on an STM32H753. The version of ThreadX being used is 6.1. I use this older version because it is ISO-62304 certified. All is functioning as desired but each time I execute code generation from CubeMX the ThreadX files are overwritten with version 6.4 (not certified). Is there any way I can avoid the update of ThreadX when I regenerate the code from CubeMX?

Thank You,

Gil

Gil1
Gil1Best answer
Associate II
Oct 31, 2025 9:48 PM UTC

Issamos,

Thank you for your quick response. I found the Software Packs Component Selector and the STMicroelectronics X-CUBE_AXRTOS-H7 component.

Gil1_0-1761944392804.png

Unfortunately, the only version is 3.3.0. I believe I need to install a previous version of the Azure RTOS expansion package.

Gil1_1-1761944652273.png

But if a previous version is installed it may not be compatible with my version of CubeMX. I believe I have to except this inconvenience.

Gil

4 replies

Issamos
Super User
Oct 31, 2025 6:37 PM UTC

Hello @Gil1 

I think you can delete the current version of the X-CUBE-AZRTOS-H7 and download the version that use the ThreadX V6.1. Also, on your .ioc file, you can go to Pinout & configuration -> Software Packs -> Select Components -> open the menu of X-CUBE-AZRTOS-H7 and select the ThreadX version you want:

Issamos_0-1761935785745.png

Sorry for the screenshot (it is not up to date).

Best Regards.

II

Gil1
Gil1AuthorBest answer
Associate II
Oct 31, 2025 9:48 PM UTC

Issamos,

Thank you for your quick response. I found the Software Packs Component Selector and the STMicroelectronics X-CUBE_AXRTOS-H7 component.

Gil1_0-1761944392804.png

Unfortunately, the only version is 3.3.0. I believe I need to install a previous version of the Azure RTOS expansion package.

Gil1_1-1761944652273.png

But if a previous version is installed it may not be compatible with my version of CubeMX. I believe I have to except this inconvenience.

Gil

Issamos
Super User
Oct 31, 2025 9:54 PM UTC

I think you should test it. If your request is answered, I think it will be better to select the comment that answered your original question as best answer to close this post.

Best Regards.

II

Gil1
Gil1Author
Associate II
Oct 31, 2025 10:06 PM UTC

In this particular project, we are very sensitive to the versions of the development software. Because of this constraint, I do not want to make this change. If a change in versions were acceptable, your solution would be fine. I will mark it so.