Skip to main content
dryet
Associate II
Sep 6, 2023 6:10 PM UTC
Solved

Using STM32 examples on custom boards

Hello,

I have made a custom board using the STM32WB55CEU6 chip and I would like to try out some examples that are available from ST. My problem is that these examples are made for STM32WB55CG and I can't find an easy way to change target of these examples. In the read me file it says:

This example has been tested with NUCLEO-G431KB RevA board and can be

easily tailored to any other supported device and development board.

But i can't seem to find an easy way to do it. 

My current aproach is:

- Getting the example project using CubeMX.

- Creating new project with the desired target

- Importing .ioc project configuration

After that I have the same configuration but the project is obviously empty. The example files are linked so i can't copy them. 

Thank you in advance for any help.

 

 

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Sep 11, 2023 2:09 PM UTC

Hello @dryet ,

I recommend you follow this FAQ: MCU1 to MCU2 migration option within STM32CubeIDE.

You can also refer to the Tutorial 5: "Exporting current project configuration to a compatible MCU" in UM1718.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Imen.DBest answer
ST Technical Moderator
Sep 11, 2023 2:09 PM UTC

Hello @dryet ,

I recommend you follow this FAQ: MCU1 to MCU2 migration option within STM32CubeIDE.

You can also refer to the Tutorial 5: "Exporting current project configuration to a compatible MCU" in UM1718.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks