Skip to main content
Associate II
Feb 27, 2025 8:58 PM UTC
Question

Using Internal Flash as Eprom at External Flash Application

Hello.

I have a custom board with STM32F750 MCU which has 64KB Internal Flash. Since the MCU's internal Flash is very limited i added external flash to board. I developed 2 different projects for Internal and External Flash. Internal Project starts with Internal Flash address. It omly includes Memory mapped init and jump codes to external Flash. External Flash Project starts with External Flash address(0x90000000). Application code stores in here.

I need r/w internal or external flash's one page or sector as a eeprom. As i know, i can't write data to external memory because it is memory mapped. Can the application code(which stored at Ext Flash), write and read internal flash?

This topic has been closed for replies.

1 reply

TDK
Feb 27, 2025 9:59 PM UTC

> Can the application code(which stored at Ext Flash), write and read internal flash?

Yes. Application code can read/write flash, doesn't matter where it's at.

"If you feel a post has answered your question, please click ""Accept as Solution""."