Skip to main content
JPark.4
Visitor II
August 16, 2018
Question

Use of ethernet after NUCLEO board cutting.

  • August 16, 2018
  • 1 reply
  • 613 views

NUCLEO board can use ST-LINK by dividing it.

Therefore, I use the ST-LINK part of the NUCLEO-767ZI and NUCLEO-207ZG boards in a divide.

After the divide, the power part and the SWD part are connected normally.

On the 207 board, Ethernet works normally but not on the 767 board.

However, if the 767 board and ST-LINK's MCO (Main Clock Output) are connected, normal operation will be performed.

207 board operates normally regardless of MCO.

Anyone who has solved the same problem as me?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
August 16, 2018

Make sure you clock configuration code uses the 16 MHz HSI rather than the missing HSE

Solder on a crystal, capacitors, and 0-ohms to the HSE (X3) locations

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..