USBX MSC SD card + FILEX SD card problem
- 9 replies
- 513 views
Hi, i'm trying to make a firmware that can read an SD card with filex but that can also connect that SD card to USBX MSC device (no simultaney).
i'm able to do the two functionality in two separate firmware, but the problem is to merge.
for now is sufficient that the card is read at start up and next i can see the SD card with USBX MSC device
when i can do that the firmware shall evolve to connect the SD card to USBX MSC and after a modification by PC disconnect the SD card the time necessary to see if something is changed and do stuff
unfortunately the first step is totally ok, at startUp i can read the SDcard with FILEX but.. after that USBX wont work
i'm using a threadX flag to indicate at the USB that is possible to use the SD card, there is some example about myu goal?
i will attach to this message the relevant files..
thank you in advance for any hint.
best reguards