Skip to main content
Visitor II
June 9, 2026
Question

USBX CDC ACM example RAM usage

Hello,

I am working with the official USBX CDC ACM example for the NUCLEO-C071RB:
https://github.com/STMicroelectronics/STM32CubeC0/tree/main/Projects/NUCLEO-C071RB/Applications/USBX/Ux_Device_CDC_ACM

Hardware: STM32C071RBT (128 KB Flash, 24 KB RAM)
Firmware: STM32Cube FW_C0 V1.4.0
Toolchain: STM32CubeIDE 2.1.1

The example runs successfully on the NUCLEO-C071RB board. However, after analyzing the RAM usage I am concerned about available headroom for my application.

Current RAM usage (from .map file):
- .data:  116 B
- .bss:   23628 B  (including ux_device_byte_pool_buffer: 8192 B, tx_byte_pool_buffer: 1024 B, three RTOS threads: 3x176 B)
- ThreadX heap (._threadx_heap in .ld): 4096 B
- Stack + Heap: 1536 B
- Total: 23744 B
- Free: 832 B (out of 24576 B)

Current configuration:
- UX_DEVICE_APP_MEM_POOL_SIZE = 8192 (app_azure_rtos_config.h)
- USBX_DEVICE_MEMORY_STACK_SIZE = 4096 (app_usbx_device.h)
- TX_APP_MEM_POOL_SIZE = 1024
- ThreadX heap in .ld = 4096 B

I need to add additional peripherals (UART, I2C, ADC) to this project which will further increase RAM usage.

My questions:
1. What are the safe minimum values for UX_DEVICE_APP_MEM_POOL_SIZE and the ThreadX heap size for a stable CDC ACM implementation?
2. Is there a recommended approach to reduce USBX + ThreadX RAM footprint on devices with only 24 KB RAM?
3. Is the standalone USBX (without ThreadX) a viable option for the STM32C071, and if so, is there a working example available?
I tried https://github.com/ST-TOMAS-Examples-USB/c071_usbx_cdc but it’t not enumerating / creating Hard Faults.

Thank you.

1 reply

ST Technical Moderator
June 9, 2026

Hi ​@luky 

I would suggest you to refer to this page explaining memory footprint in USBX and some guidelines to optimize it.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL