Skip to main content
GMeur
Associate III
July 2, 2019
Question

USBH_UserProcess never entered

  • July 2, 2019
  • 0 replies
  • 801 views

Hello,

I'm trying to use the USBH library in my project by taking the corresponding chunks of code from the USB_Host Application example present in the STM32Cube. However, I must miss an important part because the USB_UserProcess is never entered. I must add that I'm using FreeRTOS and that I call the  USBH_Process(&hUSBHost) function from within a task but it shouldn't alter the good functioning of the code normally. So, to recap briefly : I've declared two global variables :

USBH_HandleTypeDef hUSBHost;
 
 
char USBDISKPath[4]; 

Then, in the main function, before starting the scheduler or creating any FreeRTOS tasks, I've these three lines :

USBH_Init(&hUSBHost, USBH_UserProcess, 0);
 
USBH_RegisterClass(&hUSBHost, USBH_MSC_CLASS);
 
USBH_Start(&hUSBHost);

Then, I create a very simple task before starting the scheduler

xUSB = xTaskCreate(USB_Task, "USB TASK", 500, NULL, 1, NULL);

My USB task just contains a delay and the USBH_Process:

void USB_Task(void* arg)
{
 while(1){
 vTaskDelay(200);
 USBH_Process(&hUSBHost);
 }
}

And here's what's inside the USBH_UserProcess function:

static void USBH_UserProcess(USBH_HandleTypeDef * phost, uint8_t id)
{
 HAL_GPIO_WritePin(GPIOJ, LD_USER2_Pin, GPIO_PIN_SET);
}

So normally, when connecting or disconnecting a USB stick, the state of the LED should change but nothing happens. The function USBH_UserProcess is never entered by the program, although the USBH_Process function is called "every 200ms".

What am I doing wrong? What am I missing? It should be easy but I can't seem to figure out why it doesn't work.

Thanks in advance for your help.

              

               

               

                 

               

This topic has been closed for replies.