Skip to main content
VictorPr
Associate II
Sep 18, 2020 2:34 PM UTC
Solved

usbd_dfu_if.c

Hi, I'm trying to implement my own DFU bootloader interface, since I'm using a custom STM32F446RET board.

Been looking into STM32F446ZE-Nucleo DFU_Standalone project to get some ideas, but seems to be quite different to my new custom CubeMX created project.

Eg:

  • STM32F446ZE-Nucleo DFU_Standalone project has a usbd_dfu_flash.c file which contains some Flash read and write functions (Flash_If_Write, Flash_If_Read).
  • Custom CubeMX STM32F446RET board project has a usbd_dfu_if.c file, with some function prototypes like MEM_If_Write_FS, MEM_If_Read_FS

Am I supposed to write my Flash read/write code into usbd_dfu_if.c function skeletons? Makes sense, but unfortunately there is a big lack of documentation on STM32 APIs, so I better ask.

Thanks in advance

This topic has been closed for replies.
VictorPr
VictorPrBest answer
Associate II
Sep 18, 2020 11:17 PM UTC

Solved. Had to migrate old "Flash_If_xxxx" functions into "MEM_If_xxxx" function skeletons and is working now.

1 reply

VictorPr
VictorPrAuthorBest answer
Associate II
Sep 18, 2020 11:17 PM UTC

Solved. Had to migrate old "Flash_If_xxxx" functions into "MEM_If_xxxx" function skeletons and is working now.