Skip to main content
Vladimir Ermolenko
Associate II
June 19, 2018
Solved

USB vendor cpecifiq request

  • June 19, 2018
  • 1 reply
  • 873 views
Posted on June 19, 2018 at 16:09

Hi, i use STM32Cube USB device library ver. V2.2.0. My PC driver send to device vendor cpecifiq request bmRequestType = 0xC0. In UM1734 says: 'The library passes all the non-standard requests to the class-specific code with the callback pdev->pClass->Setup (pdev, req) function.' (5.1.1 -> Non-standard requests -> SETUP stage, p. 18). But realy it is not true. In file usbd_core.c this request is passed to USBD_StdDevReq and handle there as invalid.

Tell me please, this is an error in library?

#stm32cube-usb-device-library-vendor-request
This topic has been closed for replies.
Best answer by Ben K
Posted on June 19, 2018 at 18:20

Please use a brief summary of no more than 6 words as the question title.

It is hard to imagine the necessity of any control requests that need to address the USB device that this is not supported by the library. I recommend that you consider using an interface request instead, if it's fitting.

Side note: the Cube library isn't really suitable for more complex use cases - basically anything beyond the Project examples that are shipped with Cube, and it doesn't seem to be in the focus of ST software development, so don't expect much.

1 reply

Ben K
Ben KBest answer
Senior III
June 19, 2018
Posted on June 19, 2018 at 18:20

Please use a brief summary of no more than 6 words as the question title.

It is hard to imagine the necessity of any control requests that need to address the USB device that this is not supported by the library. I recommend that you consider using an interface request instead, if it's fitting.

Side note: the Cube library isn't really suitable for more complex use cases - basically anything beyond the Project examples that are shipped with Cube, and it doesn't seem to be in the focus of ST software development, so don't expect much.