Skip to main content
Associate II
Mar 25, 2026 12:48 PM UTC
Solved

USB-PD on STM32G473

Hi everyone!

I have generated a code from CubeMX for USB-PD in bare-metal configuration like this:
Screenshot 2026-03-25 134022.png  Screenshot 2026-03-25 134229.png

Then I started testing the code and the function USBPD_PE_Init at this line:

 /* PE SET UP : Port 0 */
 CHECK_PE_FUNCTION_CALL(USBPD_PE_Init(_port_index, (USBPD_SettingsTypeDef *)&DPM_Settings[_port_index], &DPM_Params[_port_index], &dpmCallbacks));

returned false.

I have looked in the assembler window and found out that some members of 

static const USBPD_PE_Callbacks dpmCallbacks =
 {
 USBPD_DPM_SetupNewPower,
 USBPD_DPM_HardReset,
 NULL,
 USBPD_DPM_Notification,
 USBPD_DPM_ExtendedMessageReceived,
 USBPD_DPM_GetDataInfo,
 USBPD_DPM_SetDataInfo,
 USBPD_DPM_EvaluateRequest,
 NULL,
 NULL, // Like this one!!!
 USBPD_PE_TaskWakeUp,
#if defined(_VCONN_SUPPORT)
 USBPD_DPM_EvaluateVconnSwap,
 USBPD_DPM_PE_VconnPwr,
#else
 NULL,
 NULL,
#endif /* _VCONN_SUPPORT */
 USBPD_DPM_EnterErrorRecovery,
 USBPD_DPM_EvaluateDataRoleSwap,
 USBPD_DPM_IsPowerReady
 };

are not allowed to be NULL. So I wonder if this is normal or I'm missing something?

THX!

FBLBest answer
ST Technical Moderator
Mar 26, 2026 10:41 AM UTC

Hi @fjahn9 

To better understand and reproduce the issue, could you please share your project setup (e.g. project files and configuration)?

If it contains confidential information, you can either send it to me in a private message or grant access to this GitHub account:: https://github.com/FBLSTM

We will treat any shared information as confidential and use it only to analyze this issue.

Thank you!

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

2 replies

FBLBest answer
ST Technical Moderator
Mar 26, 2026 10:41 AM UTC

Hi @fjahn9 

To better understand and reproduce the issue, could you please share your project setup (e.g. project files and configuration)?

If it contains confidential information, you can either send it to me in a private message or grant access to this GitHub account:: https://github.com/FBLSTM

We will treat any shared information as confidential and use it only to analyze this issue.

Thank you!

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
fjahn9Author
Associate II
Mar 26, 2026 1:53 PM UTC

Hi FBL,
thank you for your reply, but somehow during preparing the project to be sent, I regenerated the project in CubeMX one more time and now I can run my softwere without errors! I can see how software reacts on cable attachments, so this question can be marked as solved. Anyway, can you post here how to switch a Data role? I have used USBPD_DPM_RequestDataRoleSwap(PortNum) function, but nothing happened. Could you have a look at my project's files anyway?

Thank you!