Skip to main content
AOhir.1603
Associate III
January 19, 2020
Question

USB PD library gets stuck in loop waiting for VBus to be 0V when a USB-C charger plugged

  • January 19, 2020
  • 4 replies
  • 5580 views

Hi there,

We have a custom board with STM32F030CC and PTN5110 chip as the TCPC. We are using the x-cube-usb-pd library with config USBPD_TCPM_LIB_PD3_CONFIG_1.

Initially, DRP role is selected. When we plug in a standard USB-C charger (5V 3A output) to the port, TCPC reports to present Rd role. That is, in tcpc_driver->get_cc(), it returns CC_STATUS as 0x13.

But the firmware gets stuck in USBPD_DPM_IsPowerReady(), as it waits for the VBus to be 0V but the charger is presenting 5V so it gets stuck in a loop calling USBPD_DPM_IsPowerReady() (USBPD_TCPM_VBUS_IsVsafe0V() is returning USBPD_ERROR).

The firmware currently crashes after it calls USBPD_DPM_IsPowerReady() multiple times..

Could someone please help me understand why when USBPD_DPM_IsPowerReady() is called, it is waiting for VBus to be 0V in this situation? I know that VBus is actually 5V and I thought it should check to make sure VBus is 5V but library is doing the opposite.

Is there a setting I need to configure (DPM_Setting, PDO setting etc)?

Any idea would be appreciated.

Thanks,

AOF

This topic has been closed for replies.

4 replies

Yohann M.
ST Employee
January 27, 2020

Hello

Could you please attach in PD trace generated with CubeMonitor?

"For your information, we have a way to trace messages exchanged between our solution and the port partner thanks to trace mechanism.

Please have a look to the following thread: https://community.st.com/s/question/0D50X0000BdfSu2SQE/how-to-use-debug-trace-trace-

I advice you to switch to 'Consumer_RTOS' application. You could enable in this project the compilation switch _TRACE.

Then in using Cubemonitor-UCPD, you will be able to check what happens exactly.

The binary log (.cpd file) can be retrieved locally in your hard disk under:

C:\Users\<login>\AppData\Local\Temp\STM32CubeMonitor-UCPD\Acquisition

You could attach directly this file for analysis."

Regards,

Yohann

AOhir.1603
Associate III
January 27, 2020

Hi Yohann,

Thanks for your answer.

Just to clarify, I am using the USBPD_TCPM_LIB_PD3_CONFIG_1 configuration.

Could I still use the 'Consumer_RTOS' example by just changing the defined symbol to what I require it to be?

I will try and get the trace using CubeMonitor-UCPD from the application I have set up already as well.

Thanks,

AOF

Yohann M.
ST Employee
January 28, 2020

Hi AOF,

I advise you to start from EVAL_FUSB307_DRP project and disable _DRP switch (keep only _SNK switch) and then compare to 'Consumer_RTOS' project to fix different errors, mainly:

  • copy 'usbpd_pdo_defs_Snk_1Port.h' file in this application (use to define SNK PDO)
  • Few updates in 'usbpd_dpm_user.c' and 'usbpd_pwr_if.c' linked to Souce PDO and VBUS management

Please find updated files.

Regards,

Yohann

Yohann M.
ST Employee
January 28, 2020

'usbpd_dpm_user.c' and 'usbpd_pwr_if.c'  in sink only

AOhir.1603
Associate III
February 11, 2020

Hi Yohann,

I've found that the problem was the PE task having stack overflow so I've now increased the stack size from 150 to 300 in usbpd_dpm_core.c.

I found this out by adding the hook for stack overflow (vApplicationStackOverflowHook).

Now my firmware is doing what you said - restarts the state machine 3 times and then stops PD stack (PE_DISABLED_STATE)! Yeay!

But now what do I do? How do I catch this in the user code? Is there a callback I can use in usbpd_dpm_user.c to catch this scenario?

Thanks,

Ayaka

AOhir.1603
Associate III
February 17, 2020

Hi Yohann,

Thanks for clarifying the suggested solution before. I've implemented the solution with a custom timer and seems to work well.

Now, I've moved on to testing with a smart USBPD com capable charger and I have a question.

Using the same code and same charger I get different behaviour:

  1. It successfully reaches USBPD_NOTIFY_POWER_EXPLICIT_CONTRACT and can start charging my battery
  2. It seems to go through the PDO negotiation but does not reach USBPD_NOTIFY_POWER_EXPLICIT_CONTRACT. For some reason it does a Hardreset and ends up PE_DISABLED_STATE.

I've attached logs for these two cases (1. PDCharger_Working.cpd and 2. PDCharger_Hardreset.cpd).

Could you tell me why it ends up in different cases and how I could work around or fix it so it always ends up in explicit contract?

FYI I am using Nintendo switch charger to test.

Thanks,

AOF

Yohann M.
ST Employee
February 20, 2020

Hello Ayaka,

we may have on this release a system issue which leads to the fact that stack is not able to handle 2 messages coming too quickly (not able to change PE state machine after sending request message and accept message) We fixed similar issues in our latest baseline (Enable/disable RX interfaces added between the TCPM and TCPC). it allows to be sure that TCPM had the time to change its internal state machines before handle a new message..

I expect that your problem will be fixed in our next release (do our best to deliver it ASAP).

Regards,

Yohann