USB_OTG_HS isn't working on STM32H743IIT6
- September 25, 2018
- 1 reply
- 839 views
I'm trying to make work USB_HS peripheral (External PHY is USB3320). I configured CUBE project, generate code, pass 24 Mhz to USB3320 and there is nothing. Even pull up resistor that should indicate new USB device isn't working.
MCU: STM32H743IIT6 mxCube project that describes PIN connections to External Phy attached
Could anyone please provide any ideas what can cause the problem in my case?
My main culprit is:
After MS_USB_DEVICE_Init(); I have SDID bit as 1 in OTG_DCTL register but I'm sure USB_Start(); got to set this bit to zero.
P.S. I have a problems with debugger too (StLink-SWD) after I hit break-point and look at the registers (OTG1_HS_DEVICE particularly) Debugger (keil-5) show me the registers, but the next step after I have "Cannot access the target." error. I was thinking that I redefine some pins, but I doesn't. Looking at some other registers doesn't cause such problem (I tested GPIOB registers).
P.P.S How can I check that USB3320 is alive? Is there any way to make sure that this chip is correctly working?