Skip to main content
KM L.1
Associate III
December 21, 2020
Question

USB OTG FS

We are working on STM32H743BITx customized board for USB OTG FS.

We have configured the MSC but unable to detect the pendrive , nothing is getting filled in

USBDiskPath and appli_state is showing application start when pen drive is connected but its not getting active to create the file.

Thank You

Komala

This topic has been closed for replies.

3 replies

Ons KOOLI
Visitor II
December 21, 2020

Hi Komala,

Please refer to the STM32CubeH7 under Application directory.

Best Regards,

Ons.

KM L.1
KM L.1Author
Associate III
December 22, 2020

Hi Ons,

We referred the STM32CubeH7 repository code and same configuration is configured for STM32H743BITx.

The pendrive is detecting & USBdiskpath content is getting filled but unable to create the file.

I have attached the zip file of my project in keil IDE, so request you to go through it and help me out to resolve this issue.

Thank you

Komala

Ons KOOLI
Visitor II
April 9, 2021

Hi Komala,

After checking your project, I found different issues that I want to share with you:

First, I think that the SystemClock_Config is not well configured, try to use this one:

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_ClkInitTypeDef RCC_ClkInitStruct;
 RCC_OscInitTypeDef RCC_OscInitStruct;
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
 
 /*!< Supply configuration update enable */
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
 
 /* The voltage scaling allows optimizing the power consumption when the device is
 clocked below the maximum system frequency, to update the voltage scaling value
 regarding system frequency refer to product datasheet. */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 
 while ((PWR->D3CR & (PWR_D3CR_VOSRDY)) != PWR_D3CR_VOSRDY) {}
 
 /* Enable HSE Oscillator and activate PLL with HSE as source */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.HSIState = RCC_HSI_OFF;
 RCC_OscInitStruct.CSIState = RCC_CSI_OFF;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 
 /* PLL1 for System Clock */
 RCC_OscInitStruct.PLL.PLLM = 5;
 RCC_OscInitStruct.PLL.PLLN = 160;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
 HAL_RCC_OscConfig(&RCC_OscInitStruct);
 
 /* PLL3 for USB Clock */
 PeriphClkInitStruct.PLL3.PLL3M = 25;
 PeriphClkInitStruct.PLL3.PLL3N = 336;
 PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
 PeriphClkInitStruct.PLL3.PLL3P = 2;
 PeriphClkInitStruct.PLL3.PLL3Q = 7;
 PeriphClkInitStruct.PLL3.PLL3VCOSEL = RCC_PLL3VCOMEDIUM;
 PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL3VCIRANGE_0;
 
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
 PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLL3;
 HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct);
 
 /* Disable PLL3. */
 __HAL_RCC_PLL3_DISABLE();
 
 /* Select PLL as system clock source and configure bus clocks dividers */
 RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_D1PCLK1 | RCC_CLOCKTYPE_PCLK1 | \
 RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_D3PCLK1);
 
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4);
 
 /* Activate CSI clock is mandatory for I/O Compensation Cell */
 __HAL_RCC_CSI_ENABLE() ;
 
 /* Enable SYSCFG clock is mandatory for I/O Compensation Cell */
 __HAL_RCC_SYSCFG_CLK_ENABLE() ;
 
 /* Enables the I/O Compensation Cell */
 HAL_EnableCompensationCell();
}

Second, I think that the USBH_UserProcess () function is missing some code: (usb_host.c file)

/*
 * user callback definition
 */
void USBH_UserProcess (USBH_HandleTypeDef *phost, uint8_t id)
{
 /* USER CODE BEGIN CALL_BACK_1 */
 switch (id)
 {
 case HOST_USER_SELECT_CONFIGURATION:
 break;
 
 case HOST_USER_DISCONNECTION:
 Appli_state = APPLICATION_DISCONNECT;
 if (f_mount(NULL, "", 0) != FR_OK)
 {
 LCD_ErrTrace("ERROR : Cannot DeInitialize FatFs! \n");
 }
 if (FATFS_UnLinkDriver(USBDISKPath) != 0)
 {
 LCD_ErrTrace("ERROR : Cannot UnLink FatFS Driver! \n");
 }
 break;
 
 case HOST_USER_CLASS_ACTIVE:
 Appli_state = APPLICATION_READY;
 break;
 
 case HOST_USER_CONNECTION:
 if (FATFS_LinkDriver(&USBH_Driver, USBDISKPath) == 0)
 {
 if (f_mount(&USBH_fatfs, "", 0) != FR_OK)
 {
 LCD_ErrTrace("ERROR : Cannot Initialize FatFs! \n");
 }
 }
 break;
 
 default:
 break;
 }
 /* USER CODE END CALL_BACK_1 */
}

And finally, why did you choose PD3 as VBUS ?

Best REgards,

Ons.