Skip to main content
Associate
Mar 27, 2026 5:05 AM UTC
Question

USB_OTG driver development in polling based approach

Board:B-L4S5I-Iot-01A discovery kit
MCU: STM32L4s5Vit6


Hello ,

We have an application in which we are using the USB_OTG interface configured in host-only mode with the USB CDC class.

Our requirement is to receive data at a rate of once per second through this interface. However, upon configuring the USB CDC class, the USB_OTG_FS global interrupt gets enabled automatically.

In our application, we want to minimize the use of interrupts, as frequent interrupts may impact overall system performance. Therefore, we would prefer a polling-based approach, where data can be read only when required rather than being interrupt-driven.

Could you please advise if it is possible to:

  • Disable the USB_OTG_FS global interrupt, and
  • Use the USB CDC host driver in a polling-based manner to retrieve data on demand?

Any guidance or recommended approach for achieving this would be highly appreciated.

Thank you.

3 replies

gbm
Super User
Mar 27, 2026 8:06 AM UTC

It is possible to use polling for USB, it just doesn't make too much sense for any reasonable application. The statement "frequent interrupts may impact overall system performance" is not true -> actually the use of polling is what reduces the system performance.

My favorite citation from Zephyr RTOS documentation:

"Use threads to handle processing that cannot be handled in an ISR."

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
waclawek.jan
Super User
Mar 27, 2026 10:03 AM UTC

Putting aside the question of "impact overall system performance", in which I agree with @gbm :

Any system which is purely interrupt-based is very simple to convert to polled: simply poll for the flag(s) which trigger the interrupt, and if set, call the original interrupt service routine.

Whether this would work properly is another question - in case of USB host, probably yes.

JW

ST Technical Moderator
Mar 27, 2026 12:54 PM UTC

Hi  @DdAz 

I assume in device mode, you can use SOF interrupt callback associated to bInterval time base. In interrupt transfer, the host can poll the device only based on defined endpoint bInterval value, host should ensure polling at this rate.

According to STM32CubeL4 USB Host examples, the host stack always uses interrupts. I have not seen any official example of a polling only USB host driver in Cube; implementing one would likely require custom LL/HAL code.

I assume, you can start with L4 HAL to disable global interrupt here. 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL