Skip to main content
Grant Bt
Associate III
Nov 4, 2021 4:06 PM UTC
Question

USB on F103: ISRs, Disabling Interrupts and callbacks

Probably elementary stuff, but am brand new to ARM and STM32. I'm using a USB stack libusb_stm32 for learning. In this stack, when data arrives from the host PC, a callback in the USB ISR runs a function of mine to put the data into my queue. In this function of mine I have disabled interrupts, but I do NOT think I need to. Is this a correct assumption?

void Enqueue_Callback(uint8_t bytefromhost)
{
uint32_t old_primask; // VECTACTIVE is 0x24
 
old_primask = __get_PRIMASK(); // old primask was 0x0000 0000
__disable_irq(); // primask becomes 0x0000 0001
 
myenqueue(bytefromhost); // I have shared vars in here (counter, etc).
 
__set_PRIMASK( old_primask );
}

In my main code, I dequeue that data and I assume I need to disable interrupts there.

bool Dequeue(uint8_t *ch_ptr)
{
uint32_t old_primask; // VECTACTIVE is 0x00
 
old_primask = __get_PRIMASK(); // old primask is 0x0000 0000
__disable_irq(); // becomes 0x0000 0001
 
if( thereisdata() ) // <pseudocode>
 {
 mydequeue(ch_ptr); // I have shared vars in here (count, etc).
 
 __set_PRIMASK( old_primask );
 return 0;
 }
 
__set_PRIMASK( old_primask );
return 1;
}

I am used to simple 8-bit architecture where there is a single IRQ mask bit and IRQs are automatically (and visibly) masked when an ISR runs. I don't "get" the primask thing, especially in light of what I see here.

This topic has been closed for replies.

1 reply

Grant Bt
Grant BtAuthor
Associate III
Nov 8, 2021 6:33 PM UTC