Skip to main content
Alihussain Vohra
Associate III
August 18, 2020
Question

USB MSC Using SDCARD

I am using stm32f072rb discovery board. I am connecting memory card using SPI. I want to use USB MSC and want to see the SDCard data on PC. How can I do that? I used the USB_MSC_Standalone example but not working. I am attaching the code. The disk is not showing on windows but usb device is showing mass storage in device manager.

@Community member​ 

This topic has been closed for replies.

3 replies

Alihussain Vohra
Associate III
August 22, 2020

Now I am able to detect SD card on my android phone but not able to read on windows10. The speed of data transfer is very slow. How can I increase the speed of transfer?

Tesla DeLorean
Guru
August 22, 2020

SPI is likely to be quite slow, should be able to clock microsd cards between 25 to 50 MHz.

Larger sector count transfers will be more efficient.

​

There might be a MSC MEDIA PACKET SIZE define, plus you dont have a lot of RAM to buffer.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Alihussain Vohra
Associate III
August 22, 2020

Thanks @Community member​ . I will update SPI to maximum clock to 24MHz and check. I have updated MSC MEDIA PACKET to 8kb but no effect is seen on Speed of transfer. Do you have any idea about why it is not detecting on windows10?