Skip to main content
mikroforma
Associate
Jan 13, 2014 9:34 PM UTC
Question

USB MSC library bug?

Posted on January 13, 2014 at 22:34

Does anyone got USB MSC library working?  At least one suspicious place:

File:

usbd_msc_scsi.c

(...)

static int8_t SCSI_Verify10(uint8_t lun , uint8_t *params){

  if ((params[1]& 0x02) == 0x02)

  {

    SCSI_SenseCode (lun, ILLEGAL_REQUEST, INVALID_FIELED_IN_COMMAND);

    return -1; /* Error, Verify Mode Not supported*/

  }

 

  if(SCSI_CheckAddressRange(lun, SCSI_blk_addr, SCSI_blk_len) < 0)

  {

    return -1; /* error */      

  }

  MSC_BOT_DataLen = 0;

  return 0;

}

/**

* @brief  SCSI_CheckAddressRange

*         Check address range

* @param  lun: Logical unit number

* @param  blk_offset: first block address

* @param  blk_nbr: number of block to be processed

* @retval status

*/

static int8_t SCSI_CheckAddressRange (uint8_t lun , uint32_t blk_offset , uint16_t blk_nbr)

{

 

  if ((blk_offset + blk_nbr) > SCSI_blk_nbr )  //

/!!!!!!!!  <<< WHAT is here?

  {

    SCSI_SenseCode(lun, ILLEGAL_REQUEST, ADDRESS_OUT_OF_RANGE);

    return -1;

  }

  return 0;

}

(...)

The first function ''SCSI_Verify10'' calls the later one ''SCSI_CheckAddressRange'' which adds memory address in bytes to number of blocks (typical 1 block = 512 bytes) and compares to  maximum number of blocks?

May be it should be: if ((blk_offset

/ SCSI_blk_size

+ blk_nbr) > SCSI_blk_nbr )

Somebody got this example working?  ''SCSI_CheckAddressRange'' function is also used in some other SCSI processings...

Addition:

After closer look it seems that ''SCSI_Verify10'' is totally wrong (should be similar to Write10).  Fixing it ''SCSI_CheckAddressRange'' could be left as is.

Anyone from ST could confirm that? 

#usb-scsi
This topic has been closed for replies.