Skip to main content
LVall.1
Visitor II
April 30, 2020
Question

USB Mass storage and SD CARD on STM32L4R9

  • April 30, 2020
  • 0 replies
  • 687 views

Hi,

I am using the STEVAL-STWINKT1 board with STM32L4R9 MCU. I want the USB work as Mass Storage linked to 4GB SD Card, connected by SDMMC 4 bits peripheral. SD Card is formated in FAT mode. Dare are read throught FAT_FS Middleware.

It is currently working but once I connect USB to PC it takes almost 1 minute to see it on my computer device manager as a 4 GB mass storage.

The code in usbd_storage_if. has been modified as it follows

extern SD_HandleTypeDef hsd1; 
 
int8_t STORAGE_GetCapacity_FS(uint8_t lun, uint32_t *block_num, uint16_t *block_size) 
{ 
 /* USER CODE BEGIN 3 */ 
 *block_num = hsd1.SdCard.LogBlockNbr; 
 *block_size = hsd1.SdCard.LogBlockSize; 
 //*block_num = STORAGE_BLK_NBR; 
 //*block_size = STORAGE_BLK_SIZ; 
 return (USBD_OK); 
 /* USER CODE END 3 */ 
}
 
int8_t STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len) 
{ 
 /* USER CODE BEGIN 6 */ 
 HAL_SD_ReadBlocks(&hsd1, buf, blk_addr, (uint32_t) blk_len, 10); 
 return (USBD_OK); 
 /* USER CODE END 6 */ 
}
 
int8_t STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len) 
{ 
 /* USER CODE BEGIN 7 */ 
 HAL_SD_WriteBlocks(&hsd1, buf, blk_addr, (uint32_t) blk_len, 10); 
 return (USBD_OK); 
 /* USER CODE END 7 */ 
}

In debug mode, I notice the information about SD card and block size are always null. They are populated after several seconds.

Do you have any suggestions to get it faster, please?

Thank you

This topic has been closed for replies.