Skip to main content
durgesh777
Associate III
June 15, 2012
Question

USB input pins

Posted on June 15, 2012 at 12:32

Where is the USBDM and USBDP (pins name for USB) defined under standard library files from stm. I have a microcontroller with USBDM and USBDP as PA11 and PA12. I would like to know in which header file the corresonding pins are defined as USBDM and USBDP.

I would be happy if someone could help me on this.

Regards,

#usbdp #usbdm
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
June 15, 2012
Posted on June 15, 2012 at 14:24

I don't understand the question.

The pins are defined and fixed by the hardware, and the alternate function mapping.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..