Skip to main content
Fayaz.1
Associate II
August 28, 2020
Question

USB host msc stm32f107 stop writing to usb memory stick after 30-40 times. f_open() return FR_DISK_ERR

  • August 28, 2020
  • 3 replies
  • 1057 views

Hi. I'm tring to save data to usb memory stick. this is main fuction :

while (1)
 {
 /* USER CODE END WHILE */
 
 
 MX_USB_HOST_Process();
 
 /* USER CODE BEGIN 3 */
 switch(Appli_state)
 {
 case APPLICATION_IDLE:
 break;
 case APPLICATION_START:
 counter_start++;
 if(f_mount(&myUsbFatFS, (TCHAR const*)USBH_Path, 0) == FR_OK)
 {
 UsbTest_Write();
 }
 break;
 case APPLICATION_READY:
 break;
 
 case APPLICATION_DISCONNECT:
 break;
 }
 
 }

This is  UsbTest_Write(); function

bool UsbTest_Write(void)
{
 //Open or Create file for writing
 if(f_open(&myFile, "a.csv", FA_WRITE | FA_OPEN_ALWAYS ) != FR_OK)
 {
 return 0;
 }
 //Copy test Text to my temporary read/write buffer
 f_lseek(&myFile,myFile.fsize);
 sprintf(rwtext, "asdfsdfsafdfadf\tasdfsdfsafdfadf\tasdfsdfsafdfadf\n");
 //Write to text file
 res = f_write(&myFile, (const void *)rwtext, strlen(rwtext), &byteswritten);
 if((res != FR_OK) || (byteswritten == 0))
 {
 return 0;
 
 f_close(&myFile);
 }
 f_close(&myFile);
 return 1; //Success
}

When ı connect usb stick it starts to write. After write 30-40 times it stop to writing. If i disconnect usb stick and connect again. It is write again 30-40 times. I looked in debug and put break point after

UsbTest_Write()

function this time it write just 1 time and

UsbTest_Write()

function always return 0 in this line

if(f_open(&myFile, "a.csv", FA_WRITE | FA_OPEN_ALWAYS ) != FR_OK)

{

return 0;

}

Why can be this happen and how can i solve?

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
August 28, 2020

Not going to be able to debug it at the top level.

Will need to instrument the DISKIO and USB-MSC level to understand the interactions. For bus level issues a USB Analyzer

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Fayaz.1
Fayaz.1Author
Associate II
August 28, 2020

I don't understand exactly how can i do this can you explain.