Skip to main content
BParh.1
Senior III
May 10, 2021 9:37 AM UTC
Question

USB HOST MSC: Function f_findfirst() returns FR_DISK_ERR error despite USB Stick has been successfully mounted

I am trying to implement simple appication to scan existing files in USB stick in root directory. I just use ST sample as reference and following is the user call back code. The error is line 27

It manage to reach :

Appli_state = APPLICATION_START; and then successful mount f_mount().

Then it hit Appli_state = APPLICATION_READY; and then go here:

fr = f_findfirst(&dj, &fno, "/", "*.txt");

the returned fr so far always give FR_DISK_ERR. But I have verified by USB stick is ok when I use my PC to detect, write and read files.

I'd appreciate if someone can give some pointeres.

I am using STM32F769 Discovery Board and utilizing USB_OTG_HS peripheral as USB Host class MSC.

FRESULT fr; /* Return value */
DIR dj; /* Directory object */
FILINFO fno; /* File information */
 
static void USBH_UserProcess (USBH_HandleTypeDef *phost, uint8_t id)
{
 /* USER CODE BEGIN CALL_BACK_1 */
 switch(id)
 {
 case HOST_USER_SELECT_CONFIGURATION:
 break;
 
 case HOST_USER_DISCONNECTION:
 Appli_state = APPLICATION_DISCONNECT;
 printf("app disconnect\r\n");
 if(FATFS_UnLinkDriver(USBKey_Path) != 0) {
	 printf("ERROR : Cannot unlink FatFS driver! \n");
 }
 if(f_mount(NULL, "", 0) != FR_OK)
 {
	 printf("ERROR : Cannot DeInitialize FatFs! \n");
 }
 break;
 case HOST_USER_CLASS_ACTIVE:
 Appli_state = APPLICATION_READY;
 
 fr = f_findfirst(&dj, &fno, "/", "*.txt"); // why always returns FR_DISK_ERR ?
 while (fr == FR_OK && fno.fname[0]) { /* Repeat while an item is found */
 	printf("%s\r\n", fno.fname); /* Print the object name */
 	fr = f_findnext(&dj, &fno); /* Search for next item */
 }
 f_closedir(&dj);
 break;
 case HOST_USER_CONNECTION:
 Appli_state = APPLICATION_START;
 printf("app start\r\n");
 if(f_mount(&USBH_FatFs, "", 0) != FR_OK) {
	 printf("ERROR : Cannot Initialize FatFs! \n");
 }
 else {
	 printf("Mount success\r\n");
 }
 break;
 
 default:
 break;
 }
 /* USER CODE END CALL_BACK_1 */
}

This topic has been closed for replies.

1 reply

BParh.1
BParh.1Author
Senior III
May 11, 2021 2:16 AM UTC

In fact it seems, I cannot do any simple write/read too e.g. f_write() and f_read()