Skip to main content
Associate
Jan 20, 2025 9:43 PM UTC
Question

USB HOST Library certificate error stm32f405

Hi, we are developing a custom board with the STM32F405 as main micro-controller.Actually We can communicate with some flash drives and create directories and files , but with others we simply get "FR_DISK_ERR".

Some of them are detected by the Host because we can detect that current is being delivered to them, but others do nothing.

 

For example with some flash drives (Kingston) it works nice but with others It doesn't. (Doesn't matter if they are 2.0/3.0).

It seems to be relqted to the certification of each USB stick. For example

Kingston 2.0 64GB works excellent

Kingston 2.0 16GB doesn't work

Sandisk  2.0 16GB doesn't work

Kingston 64GB 3.0 works excellent 

Maybe some of them aren't original , (just clones, IDK)

All of them are formated to fat32. (Also tried exFat)

So it seems to be a problem with  uncertificated USB sticks. The question is: how can we solve it so the board can work with a huge variety of them? Is there any library or solution that improves this? Or how would  you deal with this?

 

Thanks for reading

This topic has been closed for replies.

1 reply

Associate
Jan 20, 2025 9:47 PM UTC

Add info:

*We use the usb_otg_hs port( but same problem  with FS port)

*USB host libraries are up to date

*We use fatfs library