Skip to main content
srdjan
Associate III
Jul 14, 2016 12:56 PM UTC
Question

USB double buffered endpoint question

Posted on July 14, 2016 at 14:56

Hello,

I have a CDC working with a double buffered endpoint. Everything seems fine, but I was wondering about the following situation.

When I transfer a block of data, and the last piece is <64 bytes, shouldn't the transfer terminate automatically? Instead, I see one more call to a USB interrupt (for the other buffer), and since there is no data to send, I'm sending a ZLP. After this, the transfer stops.

Even if I don't send ZLP, the data will be transferred correctly, but this extra interrupt call will be executed nonetheless.

My questions is what is the proper way to terminate the data transfer with double buffered EP?  Should I send or not this extra ZLP after a short packet, or should I just ignore this extra interrupt execution?

Also, should I call FreeUserBuffer() after this last packet or not?

Thank you,

#stm32 #usb
This topic has been closed for replies.