Skip to main content
Barbie
Associate III
April 28, 2013
Question

USB disconnect performence

  • April 28, 2013
  • 1 reply
  • 573 views
Posted on April 28, 2013 at 14:12

I have a problem when I use the USB in the Boot application and then jump to my main app without detach the USB . On the main I open it again but the other side lost connection in between. I try to stop the clock to the USB when I jump but no help.

Is there a simple way or a function that can do USB disconnect so the other side see it as the USB was disconnect?

Bar.

#usb-disconnect
This topic has been closed for replies.

1 reply

tsuneo
Associate II
April 29, 2013