Question
USB Device Virtual COM port on STM32F103RBT6 Nucleo CubeMX Keil
Posted on July 22, 2016 at 19:23
Does CubeMX supports the above?
I tried and CubeMX failed on USB selection with error, ''USB device not available. Active only when USB OTG FS IP is configure in Device mode''. There was a/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Nucleo-F103RB%20%20%2b%20USB&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=658
dated 2014. The hardware portion is still valid, right? When I download the lib 4.0.0 as the post, it advises that I should use CubeMX for new design. Is it very difficult to mix CubeMX generated HAL code with the 4.0.0 library? #usb-device-library-stm32f103rbt6 #usb-cubemx-hsi-hse-frequency