Skip to main content
Associate III
August 11, 2025
Solved

USB CoreReset stuck at count

Hi all

 

static HAL_StatusTypeDef USB_CoreReset(USB_OTG_GlobalTypeDef *USBx)
{
 __IO uint32_t count = 0U;

 /* Wait for AHB master IDLE state. */
 do
 {
 count++;

 if (count > HAL_USB_TIMEOUT)
 {
 return HAL_TIMEOUT;
 }
 } while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_AHBIDL) == 0U);

 count = 10U;

 /* few cycles before setting core reset */
 while (count > 0U)
 {
 count--;
 }

 /* Core Soft Reset */
 USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST;

 do
 {
 count++;

 if (count > HAL_USB_TIMEOUT)
 {
 return HAL_TIMEOUT;
 }
 } while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST) == USB_OTG_GRSTCTL_CSRST);

 return HAL_OK;
}

 

at the USB_CoreReset function, my code keeps on getting stuck at the count++ and doesn't progress from there. 

I have even included 

 
 RCC->AHB2ENR1 |= RCC_AHB2ENR1_OTGEN; // enable USB OTG HS clock
 RCC->AHB2ENR1 |= RCC_AHB2ENR1_USBPHYCEN; // enable ULPI clock

 

before that function call but it does nothing.
My board is stm32u5g9.

Thank you and kind regards

 

This topic has been closed for replies.
Maaz1Best answer
Associate III
August 13, 2025

The solution was 

 RCC->AHB2ENR1 |= RCC_AHB2ENR1_OTGEN; // enable USB OTG HS clock
 RCC->AHB2ENR1 |= RCC_AHB2ENR1_USBPHYCEN; // OTG_HS PHY clock enable
 RCC->APB3ENR |= RCC_APB3ENR_SYSCFGEN;

 

especially the last line of code

1 reply

Maaz1AuthorBest answer
Associate III
August 13, 2025

The solution was 

 RCC->AHB2ENR1 |= RCC_AHB2ENR1_OTGEN; // enable USB OTG HS clock
 RCC->AHB2ENR1 |= RCC_AHB2ENR1_USBPHYCEN; // OTG_HS PHY clock enable
 RCC->APB3ENR |= RCC_APB3ENR_SYSCFGEN;

 

especially the last line of code