Question
USB composite device – HID + CDC ACM example on Linux
Hello,
when using Linux host for testing this example, CDC interface is not detected by the host. Reason is sensitivity on Configuration descriptor content generated by STM32CubeMX, propagated into ux_device_descriptors.c. For now you fix this file manually if you want to verify example functionality with Linux host in ux_device_descriptors.c (~line 806)
/* Control interface headers */
pHeadDesc = ((USBD_CDCHeaderFuncDescTypedef *)((uint32_t)pConf + *Sze));
/* Header Functional Descriptor*/
pHeadDesc->bLength = 0x05;
pHeadDesc->bDescriptorType = 0x24;
pHeadDesc->bDescriptorSubtype = 0x01; //originally 0x00
pHeadDesc->bcdCDC = 0x0001; //originally 0x1001
*Sze += (uint32_t)sizeof(USBD_CDCHeaderFuncDescTypedef);Fix shall be propagated into future version of STM32CubeMX.