USB CDC receive: How do I send a NACK in order to implement flow control?
I'm using a STM32F070RB nucleo board with STM32CubeMX to implement a USB CDC device. After generating my project (and increasing the stack size minimum), I'm able to transmit data from the Windows 10 host to the CDC device by editing the CDC_Recive_FS(...) function. In this function, how do I reject the packet (sending a USB NACK) in the case that a local receive buffer is full?
My attempt is (I'm not actually storing into a local buffer... only simulating that it's full three of four times) :
static int8_t CDC_Receive_FS(uint8_t* Buf, uint32_t *Len)
{
/* USER CODE BEGIN 6 */
static int x = 0;
x++;
if((x % 4) == 1) {
USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &Buf[0]);
USBD_CDC_ReceivePacket(&hUsbDeviceFS);
uart_tx_sync(Buf, *Len);
return (USBD_OK);
} else
return (USBD_BUSY);
/* USER CODE END 6 */
}When I run this, the USB connection seems to hang. The first character is repeated on my UART, but the following characters never are sent. If I remove the "if" statement and always receive the packet, data continues being transmitted (so I think USB and such are properly setup in the firmware).
I'm using the HAL FW F0 v1.10.1.