Skip to main content
taz1000
Associate II
Dec 25, 2019 12:34 PM UTC
Solved

USB CDC in HS with STM32F405, Issue in sending data to PC.

I'm running USB CDC in HS with STM32F405.

Receiving data from PC is very good.

But, sending data to PC has problem sometimes.

To send data, I'm using CDC_Transmit_HS ( *Buf, Len )

There is no error in the function at all. But, data is not sent to PC.

To see if there is any error in CDC_Transmit_HS ( ), I checked

the hierarchical calls in CDC_Transmit_HS ().

But, even when the data is not sent, there is no error inside at all.

- Is there any known issue or possible problem that I had made ?

- Is there any relationship between USB CDC IN functions and OUT functions ?

- EX: when OUT is disabled (by not sending USBD_CDC_ReceivePacket), IN with CDC_Transmit_HS doesn't work.

* Windows10 home

* Driver for USB CDC (from device manager) : System32/Drivers/usbser.sys MS 10.0.18362.1 2006-06-21

============================================================================

Added #1.

The problem occurs when MCU sends 512 x n bytes to the host.

After an internet searching for few hours, I found articles that zero-length-packet (ZLP) is required after sending the multiple of 512 in HS mode. (in FS, it would be 64Bytes)

So, I updated CDC_Transmit_HS caller function to send ZLP if ((Len%512)==0)

( When sending ZLP CDC_Transmit_HS, return value should be checked. USBD_BUSY can be returned.)

After updating, sending any bytes of data into PC works fine.

Is this an appropriate way to fix this ?

Thanks.

This topic has been closed for replies.
thanks4opensource
Associate III
Dec 26, 2019 9:23 AM UTC

Yes, USB requires a ZLP if the last data packet in a sequence is exactly the maximum packet size for the endpoint. The end of the sequence is indicated by a short (less than max) size packet and zero works correctly.

Congratulations on finding this out after only a few hours of internet searching. It took me a lot longer than that.

I don't know what library you're using and if CDC_Transmit_HS function is part of it or from your own code. (Or if you modified CDC_Transmit_HS itself vs your calls to it). I know the ST library for the STM32F10xxx series before CubeMX generated the ZLP internally/automatically, and I'd be surprised if current CubeMX doesn't also.

1 reply

thanks4opensource
Associate III
Dec 26, 2019 9:23 AM UTC

Yes, USB requires a ZLP if the last data packet in a sequence is exactly the maximum packet size for the endpoint. The end of the sequence is indicated by a short (less than max) size packet and zero works correctly.

Congratulations on finding this out after only a few hours of internet searching. It took me a lot longer than that.

I don't know what library you're using and if CDC_Transmit_HS function is part of it or from your own code. (Or if you modified CDC_Transmit_HS itself vs your calls to it). I know the ST library for the STM32F10xxx series before CubeMX generated the ZLP internally/automatically, and I'd be surprised if current CubeMX doesn't also.