Skip to main content
Associate III
Feb 10, 2025 2:08 PM UTC
Question

USB CDC FreeRTOS Not Working after enabling the FreeRTOS

Hi team,

             I am using STM32F7 for my work, am facing one issue regarding USB CDC Class, whenever am using it without enabling this macro everything is working fine, however as soon as i enabled this macro system will stop working itself, it will not even detect the device. Is there anything additionally i need to do to enable this. 

 

#define USBH_USE_OS 1U

 

 As per my knowledge , when am not using this OS enabled USB , I am calling this USBH_Process() within infinite loop. and after enabling it , no need to call this function inside infinite loop ryt? Kindly help me to clarify these doubts. 

Regards,

Shikamaru

This topic has been closed for replies.

1 reply

ST Technical Moderator
May 13, 2025 8:48 AM UTC

Hello @Shikamaru 

You should handle the USB operations in FreeRTOS task or thread not in infinite loop. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om