Skip to main content
Dr. Ian Pratt
Associate
Dec 6, 2021 3:45 AM UTC
Question

USB CDC (Device) working with FreeRTOS on the STM32769I-DISCO. Does ST have example code of these two working together ?

I note that the XCube-AWS software employs FreeRTOS as a task scheduler. I'm using the STM32F769NI-DISCO development board to do some testing. That software is working out of the box. I can see the Ethernet handled as a task. I also see the USB CDC (Device) code for the XCube. This also works on the Discovery board. However, the USB code example does not use FreeRTOS. What steps would be needed to hook this in ? Do you have any example code using FreeRTOS and UCB CDC (Device) for this platform ?

This topic has been closed for replies.

2 replies

Walid ZRELLI
Visitor II
Dec 28, 2021 11:22 AM UTC

Hello @Dr. Ian Pratt​ ,

Unfortunately, the only available USB example with FreeRTOS if for HID and MSC **host**. The examples are located in :

  • Projects\STM32F769I_EVAL\Applications\USB_Host\HID_RTOS
  • Projects\STM32F769I_EVAL\Applications\USB_Host\MSC_RTOS

BeST Regards,

Walid

Javier1
Principal
Aug 10, 2022 8:18 AM UTC
hit me up in https://www.linkedin.com/in/javiermuñoz/