Skip to main content
danielspronk9
Associate II
April 28, 2017
Question

USB CDC Change Device name

Posted on April 28, 2017 at 12:29

Hey,

i use the STM32F4 USB CDC (generate by CUBEMX(v.4.20)) and want change the shown name in the Device Manager.

I change these lines but nothing change in the device manager.

&sharpdefine USBD_VID     1155

&sharpdefine USBD_LANGID_STRING     1033

&sharpdefine USBD_MANUFACTURER_STRING     'MyManufacture'

&sharpdefine USBD_PID_FS     22336

&sharpdefine USBD_PRODUCT_STRING_FS     'MyProduct'

&sharpdefine USBD_SERIALNUMBER_STRING_FS     '00000000005A'

&sharpdefine USBD_CONFIGURATION_STRING_FS     'CDC Config'

&sharpdefine USBD_INTERFACE_STRING_FS     'CDC Interface'

&sharpdefine USB_SIZ_BOS_DESC            0x0C

#usb_cdc
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
August 10, 2018

Sorry, bumping old zombie unanswered threads off my feed

Make sure this naming actually gets into your code. Naming may also be impacted by names associated by VID/PID in system's .INF files.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
fsha
Visitor II
March 20, 2019

If you change the const STORAGE_Inquirydata_FS in usbd_storage_if.c you can change the name of the properties/hardware. However, I also still cannot change the name from USB_Device to MyDevice. Have you made any progress there?

Tesla DeLorean
Guru
March 20, 2019

This is a two year old thread. So maybe it got fixed, or perhaps he was offered an opportunity to seek employment elsewhere..

The Inquiry Data != USB Descriptor Strings. The latter are usually UNICODE, and would need to be synthesized from ASCII strings, inspect the code building the descriptors and which are being used and generated on-the-fly vs those hard coded into structures. Inspect the binary generated by the linker to see if the data is in there.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..