Skip to main content
Ghada Dhibi
Associate II
July 27, 2017
Question

USB CDC and MSC Middlewares integration

  • July 27, 2017
  • 1 reply
  • 655 views
Posted on July 27, 2017 at 13:13

Hi all, 

I'm using STM32L486 microcontoler and USB device. 

Using MSC_Standalone and CDC_Standalone project example from the STM32Cube I was able to configure the USB device on CDC and MSC. 

Now, I want to integrate both of example on the same project, and depending on the main application, I have to choose the usb configuration to work with. 

Is there any USB device example working on both of configurations ? 

Warnings and errors occurs when I Intergate both of them. 

Thanks. 

#stm32l4 #usb #usb-cdc #usb-msc-fat #stm32l4-usb
This topic has been closed for replies.

1 reply

ST Technical Moderator
July 27, 2017
Posted on July 27, 2017 at 22:37

Hi Ghada,

Refer to this discussion, it may help you

https://community.st.com/0D50X00009Xkh8FSAR

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks