Skip to main content
YDong.11
Associate II
May 17, 2020
Question

USB Audio issues with repeat INCOMPISOOUT interrupt

  • May 17, 2020
  • 0 replies
  • 599 views

I'm having trouble implementing the Audio Device Class example from the STM32CubeMX tool on a STM32H750VBT6. 

When run, the USB appears to enumerate properly, installs the default drivers (Windows 7, btw) and shows up properly as a playback device. However, attempting to use a test tone or play through the device in any way reports a failure (no further information forthcoming).

Debugging, I can see that the USB interrupt is being triggered very often, with the flags INCOMPISOOUT (every time) .

What's the reason of INCOMPISOOUT?

And how to fix this issue?

This topic has been closed for replies.