Skip to main content
Joyabb
Associate II
Jun 29, 2020 9:04 AM UTC
Question

USB Audio Device/Host Class 2.0 Middleware support?

Hi,

I am using STM32H743 nucleo board. I am looking to configure the USB interface as Audio Class 2.0 device. Is there any middleware available to achieve this?

Does STM has any plan to support Audio Class 2.0 middleware? Current middleware only supports Audio Class 1.0.

Thanks,

Joyab

This topic has been closed for replies.

44 replies

Emmanuel_C
ST Employee
Aug 1, 2024 3:06 PM UTC

Hi guys,

One solution has been integrated in X-CUBE-AUDIO-KIT.

It supports UAC2.0 and has been used in the context of a composite device with midi, cdc, hid classes.

Robmar
Senior II
Aug 2, 2024 9:18 AM UTC

You had me hoping but sadly, as usual with STM software, it's useless, a crippled UAC 2.0 that runs at only 48 Khz, and no mention of USB support!

"Framework to support audio processing data flow

  • Up to 48 kHz

"

It forces developers to install Microsoft RTOS, which takes a lot of the limited MCU memory, and it is RTOS that has a more complete USB implementation.

Personally as a developer I am not keen on installing an OS owned by Microsoft.

Raspberry PI's industrial platform or ESP looks more attractive every day.

Emmanuel_C
ST Employee
Aug 2, 2024 9:34 AM UTC

Hi,

This package is not a USB only solution. It supports other features and has globally been validated up to 48 kHz for now. It is not a USB limitation.

By the way, this solution is not based on AzureRtos, neither USBX.

best regards

LCE
Principal III
Aug 9, 2024 5:26 AM UTC

Is it really ST's job to provide complete solutions for all and everything?
For lots of possible applications, ST provides at least a base to start from.

What are the competitors doing? Do they offer the complete "click-plug-play" package for everything?

Robmar
Senior II
Aug 9, 2024 10:02 AM UTC

You're joking right?  That STM have no viable USB driver for their MCU's without pushing people into the arms of the Microsoft, is like an electrical appliance manufacturer not using a standard power connector, and not selling that connector!

Don't you understand that if every developer has to waste time developing their own USB drivers the industry loses thousands or more hours of dev time every year for nothing.

Doing a version of TinyUSB might be a better option for STM than pushing the code heavy RTOS down clients' throats, but clearly STM do not value their MCU business, and at the rate of growth of other ARM MCU board offers, including the industrial Raspberry market, I suspect STM won't be in the market by 2030, IMHO.

MKanc.1
Associate III
Feb 27, 2025 8:41 PM UTC

Hello from 2025

Do we have 192KHz support on STM32? Using any other libraries mentioned outside ST?