Skip to main content
BErik.1
Associate
Mar 10, 2025 12:58 PM UTC
Question

USART_WakeUpFromStop1 leads to lost characters

While experimenting[*] with the USART_WakeUpFromStop1 example on my NUCLEO-L496ZG I noticed that repeatedly entering STOP1 mode leads to dropped character if running with a baudrate > 4800 bps. I'm using STOP1 mode in a different project and I hoped to find a way to correctly communicating on 115200.

Any pointers on how to achieve this?

 

[*] I had to some minor modifications to STs example

* Rewrote the reception callback to store the received bytes in an array and printout in main() instead of echoing them in the handler

void USART_CharReception_Callback(void)
{
/* Read Received character. RXNE flag is cleared by reading of RDR register */
ubReceivedChar = LL_USART_ReceiveData8(USART1);
rx_buff[rx_buff_i++] = ubReceivedChar;

/* Check if received value is corresponding to specific one : S or s */
if ((ubReceivedChar == 'S') || (ubReceivedChar == 's'))
{
...

* Removed everything not related to STOP mode from the main loop

while (ubFinalCharReceived == 0)
{
PrepareUSARTToStopMode();
EnterStop1Mode();
}
This topic has been closed for replies.

9 replies

TDK
Mar 10, 2025 9:22 PM UTC

What characters are dropped? If you wake it up by sending "Hello world" with no breaks between characters, what ends up in the rx_buff buffer after the full string is received?

"If you feel a post has answered your question, please click ""Accept as Solution""."
BErik.1
BErik.1Author
Associate
Mar 11, 2025 6:03 AM UTC

Duplicate due to moderation delay removed

Senior II
Mar 13, 2025 6:38 PM UTC

Are you changing clocks in and out of STOP?

BErik.1
BErik.1Author
Associate
Mar 14, 2025 11:39 AM UTC

Not as far as I can tell. I've never worked with the LL HAL.

 

The code is in https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Projects/NUCLEO-L496ZG/Examples_LL/USART/USART_WakeUpFromStop1/Src/main.c with a couple of minor changes as described above.

TDK
Mar 14, 2025 2:23 PM UTC

I'm not so sure this is a baud rate issue anymore. Do you get an error flags like frame error, noise error, or parity error?

Characters are dropped, but never corrupted.

Could be code going too slow to capture everything, but the drop pattern is odd.

I'm assuming the examples you sent above are actual observed results.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Senior II
Mar 14, 2025 3:24 PM UTC

What's your clock config for the USART? Clocks do change when you enter STOP. But it might not matter. I changed my clock config so stop mode would not affect the USART.

And you're not using the DMA?