Skip to main content
Senior
Jul 25, 2025 9:37 AM UTC
Solved

USART busy just after initialization

Hello,

Working on STM32F767BITx and using Free RTOS

Enable USART2, here is the init code

static void MX_USART2_UART_Init(void)
{
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_RS485Ex_Init(&huart2, UART_DE_POLARITY_HIGH, 0, 0) != HAL_OK)
 {
 Error_Handler();
 }
}

So I can see even just after init or even after some times, the gstate == 0x20 always, and thats why unable to transmit any message over uart as it is not ready.

Please guide me what is missing here.

Thanks,

Nitin

 

This topic has been closed for replies.
npatil15Best answer
Senior
Jul 25, 2025 2:35 PM UTC

Hello,

Its my mistake,

Firstly, 0x20 is a ready signal as expected, and second, I was not passing correct UART instance, which cause the communication break.

Thanks for your time

2 replies

TDK
Jul 25, 2025 2:27 PM UTC

What hardware is this one? Are the pins being pulled to their proper idle state?

"If you feel a post has answered your question, please click ""Accept as Solution""."
npatil15AuthorBest answer
Senior
Jul 25, 2025 2:35 PM UTC

Hello,

Its my mistake,

Firstly, 0x20 is a ready signal as expected, and second, I was not passing correct UART instance, which cause the communication break.

Thanks for your time