Skip to main content
JRS
Associate III
Oct 18, 2021 12:15 PM UTC
Solved

Update Schedule of HAL_Eth

Hi, is it possible to get a round-about info on the expected Hal-Eth update?

In the release notes of the Hal-Driver it is flagged as "A full rework of the ETH HAL driver is planned.." , but the last release has been in February.

I would like to avoid spending time rewriting the current driver, only to have to rewrite it again after the next release to get it back to canon again.

@Imen DAHMEN​ @Amel NASRI​ Do you maybe have the possibility to make an estimate here? E.G. in the next weeks, or within the next months, or still in tbd stage?

PS: In the Milestone for 1.10. of github I did not see any tickets regarding the driver rework.

This topic has been closed for replies.

3 replies

JRS
JRSAuthor
Associate III
Oct 22, 2021 12:27 PM UTC

As the main problem with the driver seems to the generated ethernetif.c a rework seems improbable.

My guess is based on the following:

1) no answer from ST here (only a few days, still possible :) )

2) not a lot of action in github regarding that driver for the last year.

3) a rework (using an rtos) has been suggested from allister and prepared a few years ago, but no reaction. The same for some other posts meant to sum up the current problems.

4) Current driver is also used in NetXDuo -> compatibility between lwip (ethernetif.c) and NetXDuo (nx_stm32_eth_driver.c) looks like a point that would make a rework of generation of ethernetif.c difficult.

-> So I guess in the near future there is no other way left then to get close and personal with that driver and interface, while excluding it from being overwritten by cubemx.

Pavel A.
Oct 22, 2021 7:45 PM UTC
JRS
JRSAuthorBest answer
Associate III
Dec 21, 2021 1:24 PM UTC