Skip to main content
akoluacik
Associate III
Sep 8, 2022 4:44 PM UTC
Question

Unknown type name 'HAL_StatusTypeDef' Error

Hi, I am trying to use the peripherals with their peripherals rather than initializing it with CUBEMX tool. I am only selecting 'Serial Wire' option of Debug mode under System Core -> SYS with CUBEMX. However, when I build my program, it throws the error in the title. I googled it but found nothing helpful. How can I solve this problem?

Thx in advance for your helps.

This topic has been closed for replies.

7 replies

Tesla DeLorean
Guru
Sep 8, 2022 5:06 PM UTC

Make sure you uncomment/select the modules you want in stm32f7xx_hal_conf.h

Make sure your project has "Include Paths" point to the appropriate CubeF7 directories/folders holding the include files you expect to pull in.

Make sure the command line to the compiler has USE_HAL_DRIVER and the specific IC you're using.

Perhaps review the meta-data in a working/functional project, and use that as a reference/template?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
akoluacik
akoluacikAuthor
Associate III
Sep 8, 2022 8:56 PM UTC

- I am using RTC, but do I need to enable it because I don't use HAL Library, I am using registers. I am coding in register(low) level?

- I looked at it, and everything is fine I guess, because related locations were added. I didn't mention but when I click CTRL+Left Click, I can see the definition of HAL_StatusTypeDef, but the compiler somehow cannot.

- STM32F746xx and USE_HAL_DRIVER symbols were already added.

I cannot understand the last statement/suggestion, perhaps my English isn't enough to understand. May you please make it clear? And what else do I need to check/add, or what else you can recommend?

Piranha
Principal III
Sep 11, 2022 1:09 AM UTC

> I don't use HAL Library

> USE_HAL_DRIVER symbols were already added

Don't you see anything wrong here?

> I am implementing the program with HAL Registers

First you have to understand what the HAL is and what the registers are.