Skip to main content
Andrew Neil
Super User
Jul 28, 2023 4:25 PM UTC
Question

Unhelpful documentation - LL_InitTick

eg, in stm32l0xx_ll_utils.c

 

 

/**
 * @brief This function configures the Cortex-M SysTick source of the time base.
 * HCLKFrequency HCLK frequency in Hz (can be calculated thanks to RCC helper macro)
 * @note When a RTOS is used, it is recommended to avoid changing the SysTick 
 * configuration by calling this function, for a delay use rather osDelay RTOS service.
 * Ticks Number of ticks
 * @retval None
 */

 

 

For the 'Ticks' parameter, "Number of ticks" is pretty meaningless - what is this "number"? What does it signify??

It should say, I think, "Number of ticks per second"

Thus LL_Init1msTick  does  LL_InitTick(HCLKFrequency, 1000U)  to give 1000 ticks per second - or 1 tick per millisecond.

 

This topic has been closed for replies.

6 replies

Andrew Neil
Super User
Jul 28, 2023 4:34 PM UTC

Also, the documentation fails to mention that this function (and, thus, also LL_Init1msTick) disables the SysTick interrupt.

That's an important side-effect that really needs to be noted - as can be seen from the number of forum posts about it!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Pavel A.
Jul 28, 2023 8:03 PM UTC

>Also, the documentation fails to mention that this function (and, thus, also LL_Init1msTick) disables the SysTick interrupt.

>That's an important side-effect that really needs to be noted

+1 

 

 

https://github.com/STMicroelectronics/STM32CubeL0/blob/e416b1d1ede2719bc253eb8c8029e8e338567f2f/Drivers/STM32L0xx_HAL_Driver/Inc/stm32l0xx_ll_utils.h#L222

Piranha
Principal III
Jul 29, 2023 8:58 AM UTC

And the "Number of ticks per second" can be called just "Tick frequency (Hz)". Those comments are written by the Captain Obvious, who doesn't even really understand the purpose of comments. And what is really the point of this function, when CMSIS has SysTick_Config(), which does almost the same and enables the interrupt?

By the way, don't get me wrong, but, if I would report this level of issues, there would be tens and hundreds of reports for every HAL/LL file. And that is one of the reasons I count HAL as a complete junk - fixing it or even reporting all of the issues actually requires more work than rewriting a decent driver library from the scratch.

Andrew Neil
Super User
Aug 1, 2023 5:09 PM UTC

Dear Chicken,

If you don't report the issues, you can hardly complain about there being issues.

Love,

Egg  xx.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ST Technical Moderator
Aug 3, 2023 10:21 AM UTC

Hello All,

Thank you for rising this up.

An internal ticket (ID 158538) is submitted in order to improve and avoid such issue.
PS: ID 158538 is an internal tracking number and is not accessible or usable by customers.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Andrew Neil
Super User
Aug 21, 2023 9:23 AM UTC

@Imen.D - thanks for that.

I hope this is a general ticket - not just specific to this particular function - as this type of poor-commenting is widespread.

In general, anything which involves a physical quantity should document what "units of measure" are used - in this case, "ticks per second".

And side-effects should be noted - another example here:

https://community.st.com/t5/embedded-software-mcus/hal-uart-transmit-with-single-wire-half-duplex/m-p/579685/highlight/true#M41692

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.